This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53513 with VIN<1.5V

Other Parts Discussed in Thread: TPS53513

I have an application that requires operation at 12 volts input, but also needs to run off a 1.2V input.
Vout is 0.95V @ 6.3Amps

I see the TPS53513 claims VIN is 1.5V min.
This is just the input to the drain of the top FET.

What is preventing me from putting 1.2V on VIN, 5V on Vdd to create 0.95V @ 6.3Amps?

The block diagram does not show any UVLO on VIN.

If the TPS53513 will not work do you have another solution?