This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NTC with bq27541

Other Parts Discussed in Thread: BQ27541, BQ27510, BQ27510-G2

In the datasheet of bq27541,

The thermistor circuit requires the use of an external 10-kΩ thermistor with negative temperature coefficient (NTC) thermistor with R25 = 10 kΩ ± 1% and B25/85 = 3435 kΩ ± 1% (such as Semitec 103AT) that connects
between the VCC and TS pins.


But the battery pack was picked for my design has integrated NTC that is tied to ground, can I use the NTC connection that is illustrated in the datasheet of bq27510 for bq27541 too?

Also besides bq27541, is there any other single cell fuel gauge that offers State of Health?

Best regards,

Yunfa