I need split a rail power supply for generate Vout1=+15V and Vout2=-15V. Vin=48VAC what after rectifying could be up to +68VDC. Application note SLVA369 use TPS54060 that can go up to +60VDC. Therefore I'd like to use LM5008A to be on the safe side. My question is: can I use LM5008A when main rail is inverted (negative) and positive rail is derived from coupled inductor? If not, what is an alternative?