This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063 Application Case

Hi, I am using MC34063 in my application to Convert the Voltage from 24V to 3.3 with load current 500mA.

Components used in the Circuit :

CT=100pf

L=47uH

Co=470uF

Rsc= 0.25 Ohm

Output Ripple : 20mV

Now my question is there any limitaion on the Input capacitor for this IC?

Can we use this Part directly at the Output of the powersupply ?

Eg: My application is having a Powersupply with the 48W and has got the high Output tank capacitors. ?