Dear all
Do you have maximu output current data of TPS61029.
Output : 3.3V
Input : AAA alkaline battery (1.1 - 1.7V)
Can 300 mA loading or more?
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all
Do you have maximu output current data of TPS61029.
Output : 3.3V
Input : AAA alkaline battery (1.1 - 1.7V)
Can 300 mA loading or more?
Regards,
PAN-M
you can estimate the max output current based on the equation 4 in the datasheet page 16. the peak current limit can be found at the electrical characteristic table at page 3. it is no problem for TPS61029 to support 3.3V/300mA.
thanks
Jasper Li