Hi TI,
I am using BQ24170 to design a circuit which use 13.5V-15V DC input to charge 3Cells LI-PO battery.
Refer to the data sheet description, it said the system load path can be directly connected to battery in "1 Cell application".
My questions:
1. For 3Cells LI-PO battery, is 13.5V the min supply voltage to the IC?
2. Can the system load path be directly connected to battery in "3 Cells application"? Or I only can use automatic power path selector solution in "3 Cells application"?
Many thanks.