Hello,
I was looking to see what kind of thermal management is suggested for the DCY package of the TLV1117. The regulator will be fed 5 volts, so the maximum power dissipation should be 1.36 W. (assuming (5-3.3)V*800mA)
On the data sheet the other packages have mention of connecting the pads to a spreading plane, but the DCY package has nothing mentioned. Additionally, the thermal calculator only has the option of the DRJ package. Would connecting the pad to a plane (of the same calculated size as the DRJ package) be sufficient? Or is this much management not needed?
Thanks,
Troy