Hi, I am planning to use the TPS2110A too. I want to do the OR'ing of three different Power Supplies: USB, 3.7V battery and 3.3V cell. I've studied the datasheet and seems to fit well for my purpose. However, I wanted to check with you in case I am missing something here. This is the a basic diagram of it:
-Do you recommend special in1 and in2 capacitors to avoid excessive slew rates in hot pluggable USB and LIPO Bat?
-A holdup capacitor in the output of 4.7uF should be enough for a max load of 35mA?
If you see anything I'm doing wrong or you think there is a better solution for OR'ring this, please let me know
Thanks