OKAY ON THIS PART WHAT IS THE BEST WAY TO USE THE DEADTIME CONTROL SO YOU WILL BE ABLE TO ADJUST IT
IF YOU HAVE A REF VOLTAGE ON PIN15 WHERE ARE WHAT SHOULD PINS 16 AND 1 BE DOING
IS THERE A WAY THAT I CAN MAYBE PUT A SIGNAL ON PIN 15 A TRIANGLEWAVE LETS SAY 0VDC TO 3 VDC PEAK AND USE A DC VOLTAGE ON PINS 16 AND 1 WHAN I ADJ THIS VOLTAGE UP ARE DOWN WILL IT CREATE DEADTIME OF THE OUTPUT SIGNALS
LET ME NO PLEASE ASAP
THANKS WILLIE