Hi
I want to power my circuit at 3.3v ( Current requirement max 20 MA) using single or dual alkaline cell. I have selected TPS61260 for this purpose.
so when input is as low as 1V to 1.6 V ( In single Alkaline cell ) or 1.5 V to 3.2 V ( in two cell )
my output will remain constant to 3.3v with max 20 ma. is this correct?
suggest circuit and an inductor calculations with standard part no if any.
Santosh