This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I want to control the current in the load ;
We use IGBT where the igbt frequency is low ; 8khz would be ok ; as you see in the sketch shematic we set the required current from DSP dac and compare it with current in the load via refrence resistor; then the comparator turn oFF or ON ; but we need a PWM controller that limit the switching frequency to 8khz with maximum duty cyle 100%
You may suggest other solutions too
Thank you in advanced