This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq20z95 chemistry update for Panasonic NCA103450, 2200mAh

I have to do a new project with the qp20z95. It is a battery pack with 3s1p of the Panasonic NCA103450 cell. I use the EVSW with the EV2300 HPA002.

My problem: The Panasonic NCA103450 is not in the list of chemistry selection. I know, I could do it by myself with chemistry select cycling. But I heard from a colleague in asia, that there is still a chemistry file for this cell type, with ID "2043"

I would prefer the way with the prepared file. I think, it would be more accurate and avoid mistakes.

My questions:

1. Is there still a file for the Panasonic NCA103450?

2. If there is still this file, how can I update my list in bqEASY?