This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Icc max of LM5020.

Guru 19645 points
Other Parts Discussed in Thread: LM5020

Please let me know about Icc max of LM5020.

For example,  Icc (at Vin:48V) is written on the datasheet figure-4.

But I want to know Icc at Vin:15V condition. 

 

【Supplement】

・Vcc connects to a photocoupler.

・Photocoupler's Maximum rating:20mA, Operating range:5~10 mA.

・A customer's ideal Icc is more than 20mA.

 

Best regards,

Satoshi