This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24251 temperature range

The DS for the bq2425x series specifies the recommended operating junction temperature as 0-125oC but then also gives an absolute max Tj range of -40-125oC.

Why is the recommended reduced to 0oC? If this is just the charger section then this is fine but I need to be able to draw current from the cell at temperatures down to -20oC.

I obviously accept the issues with loading Li-ion at low temperatures.

Regards.