Customer is not able to get the TPS65920 into low speed mode. He got the device in high speed mode, D+ pull-up showing. However, when he puts it into low speed mode the pullup does not change from D+ to D-. The clock is on, the ID pin is shorted low for OTG mode, all LDOs active. The ID comparitor is working.
He is writing 0x46 to register 4 for low speed mode... Is that correct? Is there something else he needs to configure 1st?
He got 0x46 from: 4 is not suspend mode, and 6 is from Tx select =2, turn-on=1, Op mode=0 (from Table 14-17. D+/D– Termination Settings Versus Signaling Mode ) in the TRM.
-Mike Score