This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2678-ADJ heats up @ 4amp



Greetings

I have made the ckt of LM2678-ADJ.

CIN1= 2200uF 35v

Cin2= 100nF ceramic

Inductor = 18uH (self made)

diode= 1n582

Cout= 100uF parallel with 33uF 16V

Input voltage is 16V @ 6 amps output voltage 13.7V @4.1 amps .... At this current ic heats up very fast.

When the load is increased it makes shrill noise and current drops.

Attached is the pcb layout made in Orcad version 9.2.

BUCK Top.pdf