Hi,
I am trying to derive a sensor node working at 3.3v using TPS63001 IC, with li-ion battery as source.
The load (node + sensor) takes a current of 200mA in active mode and 1mA in sleep mode.
When I tried to use the TPS63001 IC for regulation using the circuit configuration given in the data sheet, it was able to provide 3.3v output but the no load current was around 8mA at 3.6v input and incresed as i moved to 5 volts ot i decreased from 3.3 to 2 volts.
why this IC is taking so much current without any load?
Is there and other solution where I can get a regulated output with very low output current prefferebly in micro amps?
Thank in advance!
Shahbaz sarik