This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choosing Charger (Bq24617 vsBq24618) or (Bq25170 vs BQ24171)



Application is 3 (10.8V) or 4 (14.4V) cell 2.4Ah charger for portable instrument.  Either of these two families of products look like reasonable choices.  I need power path control and DPM.  Unit will run off of charger supply most of the time.  Unit runs off of battery until it is connected to target system under test then can run off of power provided from it.

(1) Within the families 617 vs 618 and 170 vs 171, what are the critical differences?

(2) The biggest difference between the two families seems to be internal vs external switches.  Are there other critical differences.

Thoughts from the community would be appreciated.