Hello,
Please see the attached file as Vcc current which I measured by EVM.
6574.20141128_bq24650EVM VCC current.pdf
<Q1>
Vcc current is different between pre-charge and fast-charge.
Could you please let me know this reason ?
I think that the power loss equation is "PICLOSS_Driver = VIN x Qg_total x fs".
<Q2>
Vcc current has two peaks during 1 cycle.
Where in internal circuit of bq24650 does bq24650 consume these Vcc current ?
I think that the internal 6V LDO consume the 1st peak and level shifter consume the 2nd peak.
<Q3>
Is Adapter supply current 25mA(typ) , mean of sum of current into Vcc pin?
Best Regards,
Ryuji Asaka