This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27742-G1 - Low capacity battery (45 mAh)

Other Parts Discussed in Thread: BQ27621-G1, BQ27742-G1

Hi,

We are currently using a single-cell 45 mAh battery and are looking for a suitable fuel gauge. The fuel gauge ICs I found from TI has a minimum 100 mAh capacity. I also found this post where it is suggested that a bq27621-G1 can be used by multiplying the capacity setting with 10 and then divide subsequent measures by 10.

While this would work fine for the fuel gauge functionality, I was intrigued by the integrated PCM that the bq27742-G1 features. To minimize our BOM this would be a nice feature, but I did not find any information regarding low capacity batteries.

Is it so that the bq27742-G1 does not support batteries with a capacity less than 100 mAh and that no IC that uses the Impedance Track algorithm supports the type of scaling that bq27621-G1 supports?