This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116 - 15A @ 5V. Choice of FETS.

Other Parts Discussed in Thread: LM5116

I'm wanting to use a LM5116 to get 5V@15V.  I'd like to use this driver because its in our inventory already.

I've done the numbers and it looks feasible, 

I picked a fsw of 150khz as a bit of a compromise, I have enough space to use a reasonably large indicator with low DCresistance.     I think i'll use Polycaps on the output, i need about 200uF, so ceramics just become unworkable, as they will drop to about 30% of rating with the DC bias.    4 in parallel brings the ESR down to point that is workable.

My big question really is about the choice of FETS.   The FETS i'm currently using are rated at 22A, and should do the job ok, but i was wondering if its possible to drive two FETS in parallel, which would help with the thermals for this.   Again using these FETS over other ones helps us keep inventory down.  

the smaller the number of line items in our inventory, the larger the per item Qntys get, which really helps on pricing.

I'd really appreiciate any feedback on this.