This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about UCC28950

Genius 4220 points
Other Parts Discussed in Thread: UCC28950

Hi,

I got some questions about UCC28950 as follows.

Could I ask for some advice?

(1)

if not use UCC28950 secondary sync function and Master/slave sync function,

    How should I connect these following Pins?

   8pin DELEF

   12pin DCM (to GND?)

   13pin  ADELEF (to GND?)

   16pin SYNC (open?)

   17pin OUTF (Open?)

   18pin OUTE (Open?)

(2)

Is there any limitation or ABSOLUTE MAXIMUM RATINGS for COMP pin source/Sink current?

(3)

Regarding the formula for calculating VSLOPE2 voltage,

these 2 formulas are different, which one is correct?

1.

UCC28950 600-W, Phase-Shifted, Full-Bridge Application Report

(http://www.tij.co.jp/jp/lit/an/slua560c/slua560c.pdf)

Page24 formula (146)

 2. UCC28950 Excel Design Tool_SLUC222C

(please see the attached Excel file)

the formula in "C222" cell.

Thanks

Go