This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23754EVM-383 change of resistor value



Our customer is thinking that they use EVM circuit design for their system. However they would like to use the E24 order resistor value. Thus please let me know if there is any concern about the following change.

-R13(CLS resistor): 63.4ohm ->62ohm.  Does this resistor value must be 63.4ohm +/- 1%?

-R9(FRS resistor): 69.8kohm(247kHz) -> 68kohm(253kHz). I think this is no problem.

-R11(BLNK resistor): 80.6kohm -> 82kohm. I think this is no problem.

-R12(DT resistor): 63.4kohm -> 62kohm or 56kohm. I think this is no problem.

-They would like to use DEN to Disable PoE such as the application note "SLVA306A" figure 10. They would like to use RDEN1 is 14kohm(13k + 1k (1/4W)) and  RDEN2 is 11kohm(1/10W). Is there any problem about these value?

-R22: 2.49kohm -> 2.4kohm. I think this is no problem.

-R23: 41.2kohm -> 43kohm. I think this change makes the output voltage higher.

Best Regards,

Kohei Sasaki