Other Parts Discussed in Thread: BQ24133
Hello
I want to design a charger with the BQ24133.
First question :
How works the UVLO ?
If the battery voltage (3 cells) is in a low voltage state and without any external power supply, is the BQ24133 always drive the MOSFET to the load ?
I don't see in the datasheet any stop condition about that.
The only thing I see is the UVLO but it is 3.6V and the 3 cells low voltage is about 9V.
The AVCC is directly connected to VBAT via a diode so impossible with 3 cells to reach the UVLO condition.
How to reach this condition.
Second question :
I want to use the BQ24133 to power supply the load (without any external power supply)
May I use a button to tie to ground or to the VBAT the AVCC pin ?
If AVCC is tied to ground (UVLO detect) => the power MOSFET of the Battery is not driven => no power supply to the load.
If AVCC is tied to VBAT and VBAT is not enough (see the precedent question) => the power MOSFET of the Battery is not driven => no power supply to the load
If AVCC is tied to VBAT and VBAT is enough (see the precedent question) => the power MOSFET of the Battery is driven => power supply to the load is ok
Really thanks for your quick help.
Best Regards
Jean-Marc