I am using a TPS7A3301RGWT Negative Linear Regulator in a circuit with a -17V input and -15V output. Circuit almost identical to evaluation board circuit. Using a soft-start capacitor = 1uF. Per page 10 of data sheet output settles within 40ms. In my circuit settling takes 1.6seconds. When I remove the soft start cap - regulator output stabilizes to set point per data sheet (about 40 - 50ms). Any thoughts? Thanks!