Hi,
For the TPS62125,Need urgently simulation for below requirements:
Vin= 6V-7.5V
Vout = - 5V (negative output)
Iout= 0.03A (30milly Amps) max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS62125 is supported by Webench. I suggest you use that to estimate efficiency and ripple performance. There is also an EVM available.
I don't believe webench currently supports the inverting topology, but the app note on using this device as an inverter is for a -5V out circuit and has the data you need. http://www.ti.com/lit/an/slva514b/slva514b.pdf
There's also the TPS62120/2 for this low output power.