This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can I use TPS22920 over 4A

Other Parts Discussed in Thread: TPS22920

Can I use TPS22920 over 4A

  • Hi Lionel,

     

    The maximum continuous current rating for the TPS22920 is 4A.  It can withstand higher currents for short periods of time.  The Maximum Pulsed Switch Current spec is 6A (pulse <300 μS, 2% duty cycle).

    What voltage and current rating do you need?  We have parts that support up to 15A in QFN packages.

     

    Regards,

    Adam Hoover

    DLS Applications Support 

  • Hi Lionel,

    Do you have any other questions about the TPS22920? Have you been able to determine if it will work for your design?

    Regards,
    Adam