This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV7113333 linear regulator

Other Parts Discussed in Thread: TLV711

Hello,

I am using TLV7113333 linear regulator. It has 2 outputs. And I need 200mA each on the two outputs two drive two separate circuits one consuming around 190mA and another around 80mA. Is it possible using this regulator. The datasheet doesnot mention that it can supply 200mA on each output.  Could you please clarify this confusion?

So could you kindly let me know if this regulator is capable of supplying 200mA on each of the 2 outputs?

Thank You

Nikhil