Hi,
I would like to know what is the best IC to charge and monitor one li-ion cell. At the same time i want to have an output of 3.3V. There are one IC with all of that or i need to use multiple ICs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We do not currently have a IC integrates charger and gauge together. We do have combo solutions such as the bq24250 and bq27532. The bq24532 is configured such that it can act as the master of the bq24250. However, back to your question, yes, you will need 2 ICs to acheive what you need.