This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reset IC with 2.925 V threshold, open-drain, and 6 second reset timer

Other Parts Discussed in Thread: TPS3420, TPS3897

Hi,

I'm looking for a reset IC with a reset threshold at 2.925V, open drain config.  I saw the TPS3106K33,TPS3110K33, and TPS3813K33.  The reset IC I am trying to replace has a minimum setup period for the reset input to be held low.  There is currently a 6 second period require before a reset output is triggered.  I need a supervisor IC with delayed reset output capability once a reset input (button press) is detected.  We are using this to hard-reset our device after a button is pressed for 6 seconds to be more specific.  I brought up the watchdog timer but I was told this cannot be used to solve this 6 second delay.  Any suggestions?

Thanks,

David