I want to drive a sensor node using TPS63001, all the modules in the node work at 3.3V. In active mode it takes around 150mA current and in sleep mode it takes around 80uA, the node is driven by a 3.7V, 1150mAh li-ion battery.
I got the PCB for TPS63001 using the gerber file given on TI website (TPS63000 EVM-148). I was operating it in power save mode, for some IC's the output was not remaining constant 3.3V, it was varying with the input voltage.
Some IC's were giving constant 3.3V but it was taking too much current, under no load condition it was taking current in the range 5-250mA. For some IC's they worked fine for some time i.e they were taking no load current in the range (90-300uA) but when I was testing it for different loads, at some random load condition something happened and then it also started taking very high no load current (around 120-130mA). During operation some IC's get heated very much.
During operation the IC's produces a hissing sound.
Here are a few thing which I would like to know
1. Why the IC's are behaving in this manner?
2. What can be the possible sources of error?
3. I am not using machine soldering can it be an issue?
4. I am using inductor from a local vendor instead of coilcraft, can it cause a problem?
5. What is the proper way to test a buck-boost converter?
Please let me find a way so that it works normally.
Please suggest the best buck-boost for my design, after repeated failure with TPS63001 I was planning to move to TPS63031, is it good?
Thanks in advance