Hi,
I want to charge my li-ion battery with bq24278 without system connection. As I asked earlier, you told me that SW, SYS, and BOOT components should be still connected, and left BGATE unconnected. In this case, then, should these 3 pins be still connected to VBAT? If it is so, what should I do with the MOSFET? If it is not, what should I connect the inductor? In addition, is there a special grounding requirement between AGND and PGND?
Thanks.