Hello,
I am designing a wireless acquisition system with 3V3 VCC. I have two question:
1) I would like to have the greatest time of battery. Then, What is better? Use a LDO or Switching regulator. The battery is a 3.7V. If I use a LDO the system do not work with a Vin less than 3V3 but the LDO consumption is less than switching regulator.
2)If I use a 7.4V battery, What should I use? LDO or switching regulator. The power dissipation of the LDO is (7.4-3.3)*.25mA=1.025 W, but the TPS7201 , for example, accepts a input voltage range 3V-10V.
Thanks.
Regards.