This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can TPS65070 charge 4.2V LMN cell?

Other Parts Discussed in Thread: TPS65070

Hello everyone,

According to the latest revision (G) of TPS65070 datasheet, the PMU is designed for Li-ion or Li-polymer battery. However, Li-ion is a broad class which further includes LiCoO2, LiMn2O4, LiFePO4(LMN), NMC chemistries, and it is not directly clear whether the PMU is suitable for all these subclasses.

The CHGCONFIG2 could set charge voltage in 4.1, 4.15, 4.2 and 4.25V. At least for LiFePO4 this is beyond their operating and max voltage; but for it appears that LiMn2O4 has 4.2V charging voltage. So I would like to confirm: can TPS65070 be used for LiMn2O4 cells?

 

A cross check with an article [Designing a multichemistry battery charger] by Keith Keller of TI confirms that LMN has 4.2V charging voltage. This is also in agreement with

[2] http://www.amitatech.com/Uploads/download/Cell%20spec%20download.pdf

[3] http://www.bixpower.com/Battery-Cell-Chemistry-Comparison-s/2325.htm

 

But does the CC-then-CV design of TPS65070 actually work for LMN batteries? Please give a definite Yes or No.

 

Hui