Hi, i am a final year student from NUS working on my FYP on nanocube satellite. Just recently, i have bought the High-Side MOSFET Switch TPS2031 to implement over current protection for it. I have connected the chip according to the typical application given on the datasheet, and ran a few short circuit test, however the results obtained is not the same as shown in the datasheet. can anyone help me with this?
Shorted-circuit current threshold : 0.4- 0.5 A, (not 0.6 )
output current keeps fluctuating.