I am using bq76930 evaluation module for the battery management project. On connecting through it through 10 Li ion cells. The input voltage is 25V but in the output it is showing 21V. I am not using the gauging feature. Why the output (V) is so less?
I am not using the cell gauging feature and only using the cell balancing.