I am looking for an adjustable boost regulator runs off of a VBUS input (@5V) and will have an output of 6V to 8V. The regulator will drive primarily an LED load that will often be off, but can have currents up to 50mA. I tried the TPS61080 demo board, setting the output voltage to 6V. Using a resistive load of 650 ohms it seems to work fine, with very light loads the output voltage is @ 10V. If this not the best part, can you recommend one? Here are some other requirements:
-- Need active high enable pin that set the output to 0V.
-- Max current of 50mA
-- Very stable output voltage with input variation from 4.8 to 5.2 V
-- Eficiency and footprint not too critical.
Thanks for your help,
Joe Morris
919-747-3668 x1010