Hello,
The application that is intended to be developed makes use of 20 high power infra-red LEDs. The forward voltage of each LED is 2.9V to 3.4V max, driven at a current of 1A. Now, when two sets of 10 such series LEDs are connected in parallel, the voltage that is consumed totally is 34V(max) at 2A.
Is there any LED driver that implements a Boost regulator, which can accept an input voltage of 12V, there by providing an output voltage of 34V or high with a constant current of 2A, with PWM dimming included in it?
Thanks