Hello,
My design is based on LM3409 + LED (4A) - Vin = 12V. I have used Webbench to generate the schematics. The MOSFET selected has a fast recovery body diode.
The system works well but the MSOFET gets hot very fast.
I suspect that the driver might not drive the MOSFET in saturation as expected so that the resitance might be too high - hence a power dissipation through this resistance.
I have measured PGATE (between PGATE and the Gnd) and it goes from 5 to 12V (Vin). Looking at the block diagram (in the D/S), I would say that this is expected as the Vcc is generated from Vin and the PGATE should switch from Vcc to Vin.
question 1 - When I looked at the max rating condition, I am not sure tio understand the 2nd row. Should we read PGATE max = 7V or (Vin -PGATE) = 7V max ?
Vcc being generated internally, I do not see how PGATE could be below 7V
question 2 - do you have any idea why the PMOS gets hot? any experience to share here?
best regards, Agnès