I am trying to use the TSP40170 as an adjustable current source.
If I wrap standard voltage feedback around the circuit, everything works fine. I get a regulated voltage at up to 10 amps.
If I use a high-side current sense (INA198 looking at a .003 ohm resistor) and an op-amp (LMV321) to provide the feedback, I get nothing. The FB pin measures .043V so I would expect the switcher to turn on to its maximum amount. Instead I just see an occasional narrow spike on the HDRV line and get zero current out.
Any idea what's going on?