Hi, We are using the BQ27510DRZR-G2 in a current design and it appears it is going EOL. The replacement is BQ27510DRZR-G3 and I have been told the only differences are additional pin 12 functionality and the internal oscillator frequency. What is the default configuration for pin 12? I am wondering if I can drop in the -G3 part in place of the -G2 part and it will function properly without any changes to the hardware or software interface. Does the oscillator frequency affect anything from a hardware or software interface standpoint?