This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL536A errors reset

Hi,

I have a question regarding the way to reset an error in ALERT_STATUS & FAULT_STATUS registers? 

If we detect an error via DEVICE_STATUS_REGISTER, we have a function that writes all bits of ALERT_STAUS & FAULT_STATUS registers to '1' and after that to '0' (except FORCE bits). Even if only one bit is reporting the error, we write all os them to '1' and '0'. Is it correct? Or we only have to reset the bit that is actually reporting the error?

Is there any problem if we do it so?

Thanks, 

Marina.