What is the necessary amount of on-board capacitance needed for the Vref and VTT rails out of the TPS51206DSQR. Customer is supporting two DDR3 DIMM sockets with either UDIMMs or RDIMMs.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the necessary amount of on-board capacitance needed for the Vref and VTT rails out of the TPS51206DSQR. Customer is supporting two DDR3 DIMM sockets with either UDIMMs or RDIMMs.
Hi Gary,
For stability the minimum capacitance is 10 µF on VTT and 0.22 µF on VTTREF. These should be ceramic.
This is listed in the datasheet a few times so I'm wondering if they are looking for something else?
Best Regards,
Anthony