This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can UCC28070 control from interleaved PFC to bridgeless PFC with a little additional modification?

Expert 2355 points
Other Parts Discussed in Thread: UCC28070

 

We would like to design bridgeless PFC circuit with UCC28070.

 

Condition will be as nelow:

AC Input:85-264V

DC out:400V,300W-1kW

 

There is Appnote using UCC28070 with BrridgelessPFC:

UCC28070 Implement Bridgeless Power Factor Correction (PFC) Pre-Regulator Design

http://www.ti.com/lit/an/slua517/slua517.pdf

 

 

In Appnote,it is seems to culcurate R_SYN,L1 and L2 to set current settings.

Also, it is need to achive a reduction in conducted-EMI by ttrimming R_RDM and C_CDR.

 

Should other parameters  be followed in the interleaved PFC?

 

Best regards,

 

kyt