This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2492 power limit disable

Other Parts Discussed in Thread: TPS2492, TPS2492EVM-003

Hi,

I'm using in my design TPS2492. I'm not intrest in power limit and that's why I put pull-up of 47K between VREF and PROG.

I'm using 0.1U at the timer capacitor, BSZ042N06NS for a FET and 6m Ohm for Rsh. So my current limit is 8.33A.

Vin=28V

No need for OV (tied to GND). UVEN pull-up of 100Kohm to VCC.

When loading the output at 10A (with electrical load at constant current mode) it burns the FET immediately.

At the Tina simulation (when using constant resistor at the output) I can see that it's limiting the power and after ~15mSec it turns off the FET. That might be the resion why my FET burned.

What can I do, so the TPS2492 will work as  current limit and close the FET without limiting the power on the FET.

Thanks

Shmuel

  • When using an electronic load, the constant current action can force the hotswap output below system ground (the e-load attempts to keep the current flowing even if it must reverse the output voltage to do so). If this voltage reversal exceeds -Vgs(th) of the FET, then the FET can turn back on and be damaged. You can find further description in the TPS2492 datasheet on page 25 (output clamp diode section).

    If the SOA protection feature of TPS2492 is not used, then you will need to find a larger FET that can withstand VIN (V) at ILIM (A) for Tfault time. Under the condition you describe (28V and 10A), the BSZ042N06NS can only withstand this power for ~100us at 25C.

    With Cfault = 0.1uF the fault timer will run for ~16ms which is too long for this FET. If you use the power limit feature (FET SOA protection), then you may be able to get this FET to survive this overload condition (using a resistive load which will not pull the output below ground). You can use the TI spreadsheet design tool to assist you.

    http://www.ti.com/lit/zip/slvc033

  • Eric'

    first I want to thank you for your fasr response.

    My problem is that I can’t change the package cause the board is already assembled.

    I used LT4256-1 before and I chose TPS2492 because the integrated current monitor.

    At the LT4256-1 in over current the FET transfer the current until the timer reached the timeout. The current isn’t limited.

    How can I get the same characteristics as in LT4256-1 at the TPS2492?

    I also got the TPS2492-EVM and did some tests and the results I got are very disturbing.

    I worked with pull-up of 47K between prog and vref. R3 and R5 are NA. R7 is 7 mOhm

    At constat current (7A) the FET toggled on anf off untile the timer riched 4V.

    This deosn't meet the data sheet.

    Shmuel

  • Eric,

    Typo- R7 is 10 m Ohm

  • Was the overload still applied using the electronic load? Can you try with a resistive load? Also provide scope waveforms showing the overload event. If possible, plot input voltage, output voltage, current and the timer voltage.

    In your test setup, how do you connect the input power supply to the hot swap board? Sometimes with long test cables, the input voltage can droop low enough to be below TPS2492 UVLO (~8.7V) or de-assert the EN pin. Under these conditions, the protection will not behave as expected.

  • Eric

    I attached few pictures.

    1. The setup.

    2. Evaluation Board.

    3. Power Limit- Response for constant current load (10A).

    4. Power Limit- Response for constant resistive load (1 ohm).

    At the Eval. board is with power limit (47K between PROG and VREF and 10K between PROG and GND) and the capacitor timer is 0.1uF.

    5. NO Power Limit- Response for constant current load (10A).

    6. Zoom of the above-

    7. NO Power Limit- Response for constant resistive load (1 ohm).

    At the Eval. board is without power limit (47K between PROG and VREF ) and the capacitor timer is 0.1uF.

    I hope it will help to understand the problem.

    I expected to see at the output a stady voltage until the timer reach 4V. Am I worng with my expectations?

  • Eric,

    I'm still waiting for your response.

    Thanks

    Shmuel

  • Thank you for the well detailed photos and plots. I did not see VIN droop so it seems we can rule that out. I still believe that there is an interaction with the electronic load. That is a common test problem with an active hotswap circuit. Can you try the resistive load right at the EVM output terminals and report the results? You can also just apply a direct short at the EVM output terminals if you do not have a large resistor handy.

  • Eric,

    I attached the plot of the short at the EVM output terminl:

    At my board when I did a short at the output it burn the FET. This I can't understand.

    Shmuel

  • The circuit seems to be working as expected. When the short is applied, the TPS2492 goes into current limit and the timer starts. You can see the current being regulated at the IMON pin as Vimon/Gain/Rsense or 2.4V/48/0.01 = 5A for approximately 15ms before the FET is turned off. Referring to the TPS2492EVM-003 user guide, the Q2 FET = IRF540NSPBF and figure 8 of the Q2 datasheet indicates that the 25C SOA stress applied to this FET at Vds=15V and Id = 5A should be present for less than ~10ms.

    For the case above, the stress lasted for ~15ms and exceeded the SOA of the Q2 FET.

    The TPS2492EVM-003 as designed with FET SOA protection (power limit enabled) keeps Q2 within the safe operating area when the output is shorted. Plim = Vref x R3 / (R2+R3) x 10 x Ilim = 26W. When the output is shorted, Vds = 15V and TPS2492 will regulate current at Plim / Vds = 1.74A for 16ms. This stress level for Q2 is within the SOA with plenty of margin.

    Hopefully this explanation can help to either choose a more robust FET or consider using the TPS2492 FET SOA protection feature.

     

  • Hi Eric,

    The design is already done and in the board I can't change the FET fotprint.

    Is there any way to disable the current limit of the device?

    I have a current neasurment that goes to controller, and by software I can turn off the switch when I detect over current.

    Shmuel

  • Shorting SENSE to VCC will disable current sensing.
  • Eric,

    But in that way I'll lose the current measurment.

  • Grounding the TPS2492 TIMER pin will disable the fault timer but not necessarily the current sensing. For example, for a mild overload which causes the sense voltage to exceed 50mV (but not above the fast trip threshold) the FET will fold back to regulate this current until it over-heats. Since the TIMER is disabled, TPS2492 will not turn off the FET. For more severe faults that cause the sense voltage to exceed ~100mV TPS2492 will react quickly and turn off the FET. But then TPS2492 will re-enable the FET until current limit is reached and keep it there indefinitely (until the FET overheats).