This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CEDV Fuel Gauge parameters Database

Other Parts Discussed in Thread: BQ78350, BQSTUDIO

Dear Fellows,


Is there some sort of database for CEDV parameters of known batteries? I use 8s1p battery of Tenergy 20Ah LiFePO cells (chemistry ID 0x0431) with bq78930EVM (bq78350 gas gauge); do I need to perform experiments described in SLUUB45, or I can somehow else get this data?  As far as I understand it is supposed to be parametrization of a whole stack, which should be possible to derive from single cell data - hence available for chemistries known to bqStudio.

I ask for this matter, because when I update chemistry via bqStudio, there is no change in flash memory parameters I read from device - especially not in CEDV Cfg section - those values remain as default ones of LiCoO2 cell.

Best regards,

Mike