Hi
I'm using TPS62740 and found the power consumption in bypass mode without load is strange.
Applicaiton usage:
1. Set output voltage to be 3.3 V with programing setting to the input signals.
2. Without load
Current test result:
Case 1: ramp up the VIN from 0.1 V to 3.4 V, the VOUT will follow the input, the current is about 16 uA.
Case 2: ramp up the VIN from 3.4 V to 4.5 V, the VOUT is fixed to 3.3 V and the current is 1 uA ~ 6uA.
Case 3: ramp down the VIN from 4.5 to 3.4 V, the VOUT is fixed to ~ 3.3 V and the current is 1 uA ~6 uA.
Case 4: ramp down the VIN from 3.4 V to 2.5V, the VOUT will follow the input with 0.1 V loss and the current is about 280 uA.
Why the current in case 4 is that much? Is there something wrong?
Regards
Jin