This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Replacement for Bq28z560-R1

Other Parts Discussed in Thread: BQ27742-G1, BQ34Z100

We started and put on hold a design using BQ28Z560-R1 as the gas gauge (pack side) for a large capacity battery pack (20k+ mAh).  This battery is now being re-instated.  However, BQ28Z560-R1 is now NRND, and in the forum, it is suggested that BQ27742-G1 be used instead.  However, BQ27742-G1 is only for cell capacity of up to 16,000 mAh.  Is there another gas gauge that will support larger capacity than the BQ27742-G1?  From the listing of gas gauges in the catalog, BQ34Z100 is a potential candidate, however is there something more suitable?

Thanks.