This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about design circuit of TPS386000

Guru 19655 points


Customer design following circuit.

※Vsense:①+5.0V、②+3.3V、③+4.5V

 ⇒Vth:①+4.5V、②+2.9V、③+4.2V

【Problem】

Though the Vsense voltage of everything exceeds Vth (5V or 3.3V), a reset signal is a condition of "Low".

Is there a mistake in a circuit diagram?

(Are MR, CT and Watchdog OK?)

Please let me know.

 

Best regards,

Satoshi