This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Non isolated solution for 60V~84V DC input to 15V output



Hi All,

Our customer looking for non isolated solution for following power requirement. Can you introduce suitable device or reference design?

Input voltage : 60V~84V DC (20 series Li-Ion battery), 100V input voltage range is needed for device

Output voltage : 15V

Output current : 1A

Other : They do not need isolation but they need 100V input voltage range for device, so they think TI do not have non-isolated solution for this requirement.

Best Regards,

Sonoki / Japan Disty